MQX 4.2 Cloning Wizard Name Size Limit?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MQX 4.2 Cloning Wizard Name Size Limit?

ソリューションへジャンプ
1,636件の閲覧回数
gorakk
Contributor IV

Is there a size limit for the Name of a cloned BSP?

I originally put a fairly long descriptive name for a new BSP - but when I tried to generate the project an error was shown.

For example - if I use a Name of: abcdefghijklmnopqrstuvwxyz0123456789

The following error is shown:

C:/Users/allwel/AppData/Local/Temp/ocr3A43.tmp/src/core/uproject/internal/_xml_utils.rb:21:in `initialize': No such file or directory @ rb_sysopen - ../../../mqx/examples/context_switch_callback/build/kds/context_switch_callback_abcdefghijklmnopqrstuvwxyz0123456789/context_switch_callback_abcdefghijklmnopqrstuvwxyz0123456789 int flash release jlink.launch (Errno::ENOENT)

Something shorter - abcdefghijklmnopqrstuvwxyz - will work ok.

Is there meant to be a size limit?

Regards,

Allen

タグ(2)
0 件の賞賛
返信
1 解決策
1,517件の閲覧回数
soledad
NXP Employee
NXP Employee

Hello Allen,

Only 32 characters can be used for the name.


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,518件の閲覧回数
soledad
NXP Employee
NXP Employee

Hello Allen,

Only 32 characters can be used for the name.


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信