MQX 4.2 Cloning Wizard Name Size Limit?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

MQX 4.2 Cloning Wizard Name Size Limit?

跳至解决方案
1,640 次查看
gorakk
Contributor IV

Is there a size limit for the Name of a cloned BSP?

I originally put a fairly long descriptive name for a new BSP - but when I tried to generate the project an error was shown.

For example - if I use a Name of: abcdefghijklmnopqrstuvwxyz0123456789

The following error is shown:

C:/Users/allwel/AppData/Local/Temp/ocr3A43.tmp/src/core/uproject/internal/_xml_utils.rb:21:in `initialize': No such file or directory @ rb_sysopen - ../../../mqx/examples/context_switch_callback/build/kds/context_switch_callback_abcdefghijklmnopqrstuvwxyz0123456789/context_switch_callback_abcdefghijklmnopqrstuvwxyz0123456789 int flash release jlink.launch (Errno::ENOENT)

Something shorter - abcdefghijklmnopqrstuvwxyz - will work ok.

Is there meant to be a size limit?

Regards,

Allen

标记 (2)
0 项奖励
回复
1 解答
1,521 次查看
soledad
NXP Employee
NXP Employee

Hello Allen,

Only 32 characters can be used for the name.


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,522 次查看
soledad
NXP Employee
NXP Employee

Hello Allen,

Only 32 characters can be used for the name.


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复