MQX 4.2.0 support of SPI Fast continuous Mode for Vybrid VF61?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MQX 4.2.0 support of SPI Fast continuous Mode for Vybrid VF61?

701 次查看
davidwightman
Contributor II

Is it possible to use the fast continuous mode with Vybrid VF61 SPI in MQX?

It seems like there are no hooks to ensure that the SPIx_PUSHR configuration bits are set or even maintained within the SPI driver. 

0 项奖励
回复
1 回复

593 次查看
Carlos_Musich
NXP Employee
NXP Employee

Hi David,

this mode is not supported, sorry for the inconvenience.

Carlos

0 项奖励
回复