MQX 4.2.0 support of SPI Fast continuous Mode for Vybrid VF61?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MQX 4.2.0 support of SPI Fast continuous Mode for Vybrid VF61?

468 Views
davidwightman
Contributor II

Is it possible to use the fast continuous mode with Vybrid VF61 SPI in MQX?

It seems like there are no hooks to ensure that the SPIx_PUSHR configuration bits are set or even maintained within the SPI driver. 

0 Kudos
Reply
1 Reply

360 Views
Carlos_Musich
NXP Employee
NXP Employee

Hi David,

this mode is not supported, sorry for the inconvenience.

Carlos

0 Kudos
Reply