MQX 4.1.1 I2C Driver

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

MQX 4.1.1 I2C Driver

跳至解决方案
1,068 次查看
josephchen
Contributor III

I'm using MQX 4.1.1 and working on I2C example. When I use I2C interrupt, it's calling the low level driver functions in i2c_int_ki2c_legacy.c file. If I try to replace with i2c_int_ki2c.c file, there're will be some macros undefined, for example I2C_FLT_SSIE_MASK in the line 129, and some others. I wonder if there's anyone using the one which is not legacy in MQX 4.1.1.

1 解答
935 次查看
danielchen
NXP TechSupport
NXP TechSupport

Hi Joseph:

Please check the i2c driver for bsp_twrk64f120m,  it uses i2c_int_ki2c.c file, not i2c_ki2c_legacy.c


Have a great day,
Daniel

在原帖中查看解决方案

0 项奖励
回复
1 回复
936 次查看
danielchen
NXP TechSupport
NXP TechSupport

Hi Joseph:

Please check the i2c driver for bsp_twrk64f120m,  it uses i2c_int_ki2c.c file, not i2c_ki2c_legacy.c


Have a great day,
Daniel

0 项奖励
回复