I'm using MQX 4.1.1 and working on I2C example. When I use I2C interrupt, it's calling the low level driver functions in i2c_int_ki2c_legacy.c file. If I try to replace with i2c_int_ki2c.c file, there're will be some macros undefined, for example I2C_FLT_SSIE_MASK in the line 129, and some others. I wonder if there's anyone using the one which is not legacy in MQX 4.1.1.
已解决! 转到解答。
Hi Joseph:
Please check the i2c driver for bsp_twrk64f120m, it uses i2c_int_ki2c.c file, not i2c_ki2c_legacy.c
Have a great day,
Daniel