MQX 3.8 _time_get() ->_time_to_date defect

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MQX 3.8 _time_get() ->_time_to_date defect

3,889 次查看
timias
Contributor IV

I noticed the following behavior in my code using the MQX 3.8 and the  K60 BSP -didn't confirm other processors

occasionally the following pair of calls will fail, and the _time_to_date function will return FALSE. Though you wouldn't notice it since most MQX internal calls ignore the _time_to_date function return value. This seems to be the source of a ton of file time stamp glitches I have noticed.

I was using the following code and had to change it, but the problem still exist all over MQX. I will probably patch MQX myself.

_time_get(&time_mqx);

_time_to_date(&time_mqx, &clk_time);

My fix for the snippet was :

_time_get(&time_mqx);

/* Fix for a wonderful little MQX bug*/

    if (time_mqx.MILLISECONDS ==1000){

   time_mqx.MILLISECONDS =0;
   time_mqx.SECONDS++;

    }

_time_to_date(&time_mqx, &clk_time);


   
10 回复数

2,568 次查看
timias
Contributor IV

FYI the fix was NOT included in MQX 4.0

0 项奖励
回复

2,568 次查看
BielikM
Contributor III

FYI: the fix has been applied and will be included in MQX 4.0.1 release.

2,568 次查看
billnd
Contributor IV

Any hint as to when 4.0.1 will be released?

0 项奖励
回复

2,568 次查看
BielikM
Contributor III

Ideally 22.4.2013.

0 项奖励
回复

2,568 次查看
JuroV
NXP Employee
NXP Employee

Hi Robert,

you are right. On the other hand there are plans and already some progress in remaking timer concept in MQX.

0 项奖励
回复

2,568 次查看
c0170
Senior Contributor III

Hello,

yes, it's not in MQX 4.0 as you stated. This will be fixed but first this bug requires thorough code review and perhaps to rewrite more parts of the code :smileywink:

Regards,

MartinK

0 项奖励
回复

2,568 次查看
c0170
Senior Contributor III

Hello Robert,

Thank you for reporting the bug, I will dig into it during this week and I will return here with an outcome.

Regards,

MartinK

0 项奖励
回复

2,568 次查看
c0170
Senior Contributor III

Hello,

can you replace function _psp_ticks_to_time in psp_tkti.c and rebuild psp and test this:

  boolean _psp_ticks_to_time

   (

      /* [IN] Pointer to the tick struct to store the results in */

      PSP_TICK_STRUCT_PTR tick_ptr,

      /* [OUT] Pointer to the time struct to convert */

      TIME_STRUCT_PTR     time_ptr

   )

{ /* Body */

   uint_64                tmp, hwt;

   uint_32                tps;

   KERNEL_DATA_STRUCT_PTR kernel_data;

   _GET_KERNEL_DATA(kernel_data);

   tps = kernel_data->TICKS_PER_SECOND;

   /* Saturate if ticks go out of range of time struct */

   if ( (tick_ptr->TICKS[0] / tps) > MAX_UINT_32) {

      time_ptr->SECONDS      = MAX_UINT_32;

      time_ptr->MILLISECONDS = 999;

      return FALSE;

   } /* Endif */

   /* */

   tmp = (tick_ptr->TICKS[0] * 1000) + (tick_ptr->HW_TICKS[0] * 1000 / kernel_data->HW_TICKS_PER_TICK);

   tmp = tmp / tps;

   time_ptr->SECONDS      = tmp / 1000;

   time_ptr->MILLISECONDS = tmp - time_ptr->SECONDS * 1000;

   return TRUE;

} /* Endbody */



Regards,

MartinK


2,568 次查看
audi_mcavoy
Contributor IV

MartinK -- That seems to have fixed the problem for me too.  Thanks!

0 项奖励
回复

2,568 次查看
timias
Contributor IV

That seemed to solve my problem, without adding any discernible side effects.

Thanks for the help

0 项奖励
回复