MAC address

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MAC address

Jump to solution
2,617 Views
vines
Contributor III

Hi All,

It seems that the MAC address for the MQX is generated depending on the parameters you pass it into.

ENET_get_mac_address(ENET_DEVICE, ipDataGlobal.ip, tempMAC);

Isn't suppose to be a running number based from the manufacturer? If no, can I just use any generated running number here and not worry about licenses or something?

Thank You.

1 Solution
1,877 Views
ivanpajuelo
Contributor II

For testing you can use the MAC address you want.

For production you need to acquire a MAC range. Follow this link IEEE-SA - Registration Authority OUI

Some MCUs already have a registered MAC address of the manufacturer you can use.

View solution in original post

2 Replies
1,877 Views
Martin_
NXP Employee
NXP Employee

Ivan is right, just would like to add the function which should be modified for production: _bsp_get_mac_address() function in your BSP (init_enet.c source file).

1,877 Views
ivanpajuelo
Contributor II

For testing you can use the MAC address you want.

For production you need to acquire a MAC range. Follow this link IEEE-SA - Registration Authority OUI

Some MCUs already have a registered MAC address of the manufacturer you can use.