MAC address

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

MAC address

跳至解决方案
2,537 次查看
vines
Contributor III

Hi All,

It seems that the MAC address for the MQX is generated depending on the parameters you pass it into.

ENET_get_mac_address(ENET_DEVICE, ipDataGlobal.ip, tempMAC);

Isn't suppose to be a running number based from the manufacturer? If no, can I just use any generated running number here and not worry about licenses or something?

Thank You.

1 解答
1,797 次查看
ivanpajuelo
Contributor II

For testing you can use the MAC address you want.

For production you need to acquire a MAC range. Follow this link IEEE-SA - Registration Authority OUI

Some MCUs already have a registered MAC address of the manufacturer you can use.

在原帖中查看解决方案

2 回复数
1,797 次查看
Martin_
NXP Employee
NXP Employee

Ivan is right, just would like to add the function which should be modified for production: _bsp_get_mac_address() function in your BSP (init_enet.c source file).

1,798 次查看
ivanpajuelo
Contributor II

For testing you can use the MAC address you want.

For production you need to acquire a MAC range. Follow this link IEEE-SA - Registration Authority OUI

Some MCUs already have a registered MAC address of the manufacturer you can use.