Is it possible to change the MQX 4.0 root directory?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is it possible to change the MQX 4.0 root directory?

Jump to solution
1,136 Views
cavebiker
Contributor V

Is it possible to change the MQX 4.0 root directory or install it to a different place?

This is a configuration management thing, no biggie if it can’t be done. MQX Rocks---

Cheers,

Tom


0 Kudos
Reply
1 Solution
1,003 Views
cavebiker
Contributor V

Thanks Kojto,

I needed to do an uninstall and install, that did it :smileycool:

Cheers

View solution in original post

0 Kudos
Reply
2 Replies
1,003 Views
c0170
Senior Contributor III

Hello Tom Junkans,

yes, it allows you to install it to specific directory.

Regards,

MartinK

0 Kudos
Reply
1,004 Views
cavebiker
Contributor V

Thanks Kojto,

I needed to do an uninstall and install, that did it :smileycool:

Cheers

0 Kudos
Reply