Is it possible to change the MQX 4.0 root directory?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Is it possible to change the MQX 4.0 root directory?

ソリューションへジャンプ
1,186件の閲覧回数
cavebiker
Contributor V

Is it possible to change the MQX 4.0 root directory or install it to a different place?

This is a configuration management thing, no biggie if it can’t be done. MQX Rocks---

Cheers,

Tom


0 件の賞賛
返信
1 解決策
1,053件の閲覧回数
cavebiker
Contributor V

Thanks Kojto,

I needed to do an uninstall and install, that did it :smileycool:

Cheers

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,053件の閲覧回数
c0170
Senior Contributor III

Hello Tom Junkans,

yes, it allows you to install it to specific directory.

Regards,

MartinK

0 件の賞賛
返信
1,054件の閲覧回数
cavebiker
Contributor V

Thanks Kojto,

I needed to do an uninstall and install, that did it :smileycool:

Cheers

0 件の賞賛
返信