Include ARM CMSIS DSP in project MQX

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Include ARM CMSIS DSP in project MQX

1,459 次查看
feraro
Contributor IV

Hello.

I have a project based in MQX 3.7, I`m using Codewarrior 10.5 and cpu MK60DN512. Can I add in my project the libraries ARM CMSIS DSP?. Can someone guide me on how to do?

Thank you.

0 项奖励
回复
2 回复数

1,187 次查看
soledad
NXP Employee
NXP Employee

Hello Fer,

Please check the below application note, this appnote discusses the CMSIS DSP library combined with Freescale MQX RTOS.

http://cache.freescale.com/files/microcontrollers/doc/app_note/AN4489.pdf


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,187 次查看
feraro
Contributor IV

Hello Sol.

Thanks for your answer.
Had seen this note alpicacion, but it explains how to implement it in IAR and I am using CodeWarrior 10.5.

I Tried to add the libraries in the CodeWarrior, in ARM Compiler and ARM Linker, but when compiling the project many errors in the file arm_math.h


Best regards.


Fernando.

0 项奖励
回复