Include ARM CMSIS DSP in project MQX

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Include ARM CMSIS DSP in project MQX

1,028 Views
feraro
Contributor IV

Hello.

I have a project based in MQX 3.7, I`m using Codewarrior 10.5 and cpu MK60DN512. Can I add in my project the libraries ARM CMSIS DSP?. Can someone guide me on how to do?

Thank you.

0 Kudos
Reply
2 Replies

756 Views
soledad
NXP Employee
NXP Employee

Hello Fer,

Please check the below application note, this appnote discusses the CMSIS DSP library combined with Freescale MQX RTOS.

http://cache.freescale.com/files/microcontrollers/doc/app_note/AN4489.pdf


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

756 Views
feraro
Contributor IV

Hello Sol.

Thanks for your answer.
Had seen this note alpicacion, but it explains how to implement it in IAR and I am using CodeWarrior 10.5.

I Tried to add the libraries in the CodeWarrior, in ARM Compiler and ARM Linker, but when compiling the project many errors in the file arm_math.h


Best regards.


Fernando.

0 Kudos
Reply