How to set SDHC clock to 50MHz?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

How to set SDHC clock to 50MHz?

跳至解决方案
3,591 次查看
naftalir
Contributor III

Hi,

I've tested the SDCLK and noticed it works default in 20MHz clock, so i've managed to chage it to 40MHz but not to 50MHz.

My code looks like that:

        /* Set SDCLK to 40Mhz*/

        esdhc_ptr->SYSCTL &= 0xFFFFFFF7; //Disable the SD Clock

        esdhc_ptr->SYSCTL &= 0xFFFF00FF; //Setting the Prescaler to 0

        esdhc_ptr->SYSCTL |= 0x00000020; //Setting the Divisor to 3 

        esdhc_ptr->SYSCTL |= 0x00000008; //Enable the SD Clock

        esdhc_ptr->SYSCTL |= 0x00000004; //Remain the SDHC clock always enabled 

标记 (3)
0 项奖励
回复
1 解答
2,858 次查看
c0170
Senior Contributor III

Hello,

SIM_SOPT2[SDHCSRC] register specifies Clock for SDHC peripheral. I note that you did not clarify your target MCU, therefore everything what I have written is for K40. Slight changes might be for different MCU.

Regards,

MartinK

在原帖中查看解决方案

0 项奖励
回复
10 回复数
2,859 次查看
c0170
Senior Contributor III

Hello,

SIM_SOPT2[SDHCSRC] register specifies Clock for SDHC peripheral. I note that you did not clarify your target MCU, therefore everything what I have written is for K40. Slight changes might be for different MCU.

Regards,

MartinK

0 项奖励
回复
2,858 次查看
naftalir
Contributor III

Again, Thank you for your true help! :smileyhappy:

I forgot to mention my MCU: K60F120M, if there is any change to what you wrote i will be happy to know :smileyhappy:

Sincerely yours,

Naftali.

0 项奖励
回复
2,858 次查看
MarkP_
Contributor V

Hi,

I created a test project with CW 10.2 and selected PE-support.

The configuration is shown in picture below and register initialization is in attached C-file.

~Mark

.MK60_config.png

2,858 次查看
naftalir
Contributor III

Hi Markku!

Thank you for your help.

I did managed to get 50MHz with the source of the OSC0ERCLK:

/* My Code for this is: */

SDHC_MemMapPtr esdhc_ptr = SDHC_BASE_PTR; 

SIM_MemMapPtr sim_ptr = (SIM_MemMapPtr)0x40047000; //Base address of the SIM

/* Set the SDHC clk source to OSC0 = 50MHz */

sim_ptr->SOPT2 |= 0x20000000; //Set ESDHCSRC clk to OSC0ERCLK

esdhc_ptr->SYSCTL &= 0xFFFF00FF; //Disable the Prescaler

esdhc_ptr->SYSCTL &= 0xFFFFFF0F; //Disable the Divisor 

Thank you all for your help: Kojto and Markku!!

:smileyhappy:

0 项奖励
回复
2,858 次查看
MarkP_
Contributor V

I think 50MHz cannot be generated from 120MHz CPU clock, need to be 100MHz.

0 项奖励
回复
2,858 次查看
naftalir
Contributor III

****I've accidently pressed "Send Button".

My question is: how to set the registers in order to provide clock of 50MHz, when the CPU Clock is 120MHz?

Thank you all.

0 项奖励
回复
2,858 次查看
c0170
Senior Contributor III

Hello naftalir,

I assume you are using Kinetis platform. There''s section in Reference Manual for your MCU where this equation is written:

Clock frequency = Base clock / (prescaler x divisor)

There's not much to do here to set desired 50 MHz with 120 MHz source clock. Closest you can get is 40 MHz. You can anyway change the bus clock.

Regards,

MartinK

0 项奖励
回复
2,858 次查看
naftalir
Contributor III

Thank you Kojto,

If i change the bus clock it will change the whole system performance..

Can i do it somehow without affected the system?

0 项奖励
回复
2,858 次查看
c0170
Senior Contributor III

Hello,

I forgot to mention, there's chapter in Reference manual dedicated to Clock distribution with the same name.

This is based on Kinetis 40:  There're 4 possible clock sources :

System clock

MCGPPLLCLK/MCGFLLCLK

OSCERCLK

SDHC0_CLKIN

You can select one of these clock sources for SDHC module and customize divider to have 50 MHz.

Regards,

MartinK

2,858 次查看
naftalir
Contributor III

Again, Thank you Kojto but may i ask you for example on how to change the clock source?

i cant seem to find it..

Thank you.

0 项奖励
回复