How many RAM(KB) MQX RTCS uses?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How many RAM(KB) MQX RTCS uses?

ソリューションへジャンプ
2,617件の閲覧回数
Chuki
Contributor I

Hi there,:smileyhappy:

 

How many RAM(KB) MQX RTCS uses?

 

I have a plan to develop a IP still image camera system using MCF5225x.

I want to know that I have to add external RAM or not.

 

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
1,909件の閲覧回数
admin
Specialist II

The amount of RAM RTCS uses is highly dependant on how you configure it. That is: what protocols you use, how large you make the various queues and memory partitions, etc.

 

 

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,909件の閲覧回数
ordnajelAlejand
Contributor I

Hey chuki, I have the same question as you, if you get the anwer please post it! 

0 件の賞賛
返信
1,910件の閲覧回数
admin
Specialist II

The amount of RAM RTCS uses is highly dependant on how you configure it. That is: what protocols you use, how large you make the various queues and memory partitions, etc.

 

 

0 件の賞賛
返信