How many RAM(KB) MQX RTCS uses?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How many RAM(KB) MQX RTCS uses?

Jump to solution
2,636 Views
Chuki
Contributor I

Hi there,:smileyhappy:

 

How many RAM(KB) MQX RTCS uses?

 

I have a plan to develop a IP still image camera system using MCF5225x.

I want to know that I have to add external RAM or not.

 

Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
1,928 Views
admin
Specialist II

The amount of RAM RTCS uses is highly dependant on how you configure it. That is: what protocols you use, how large you make the various queues and memory partitions, etc.

 

 

View solution in original post

0 Kudos
Reply
2 Replies
1,928 Views
ordnajelAlejand
Contributor I

Hey chuki, I have the same question as you, if you get the anwer please post it! 

0 Kudos
Reply
1,929 Views
admin
Specialist II

The amount of RAM RTCS uses is highly dependant on how you configure it. That is: what protocols you use, how large you make the various queues and memory partitions, etc.

 

 

0 Kudos
Reply