H-Files not moved after compiling the BSP

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

H-Files not moved after compiling the BSP

跳至解决方案
1,129 次查看
demheld
Contributor I

Hello everybody

When I compile my (ported) BSP the Processor Expert Files are not moved into the

{MQXRootDir}\lib\MyOwnBSP\debug\bsp\Generated_Code  and

{MQXRootDir}\lib\MyOwnBSP\debug\bsp\Sources

which then throws an Error while compiling the actual project saying it couldn't find the corresponding h-files.

So all the components from PEx are not seen.

I am, for now, copying all the h-files manually from

{MQXRootDir}\mqx\build\cw10gcc\MyOwnBSP\Generated_Code

{MQXRootDir}\mqx\build\cw10gcc\MyOwnBSP\Sources

to

{MQXRootDir}\lib\MyOwnBSP\debug\bsp\Generated_Code  and

{MQXRootDir}\lib\MyOwnBSP\debug\bsp\Sources

I don't really understand where exactly I messed up during my BSP porting procedure and what i have to fix.

Is it the make Files? Or the MyOwnBSP.bat file? I tried comparing with a running ported BSP (almost the same) and couldn't find

the issue.

It would be lovely if someone pointed me into the right direction where to find the mistake.

cheers

标签 (1)
0 项奖励
回复
1 解答
985 次查看
demheld
Contributor I

Hi

Thanks for the answer.

Those two commandlines are there and also the files are copied.

On top of that I even have the two lines which shoud exactly copy my desired files:

It is a bit strange because with one of my ported BSPs it is working and with one it's not, even though it looks good to me in

both cases.

Copying files is working:

for /R "%ROOTDIR%\mqx\build\cw10gcc\bsp_RSc_K20\Generated_Code" %%f in (*.h) do copy %%f "%OUTPUTDIR%\Generated_Code\"

for /R "%ROOTDIR%\mqx\build\cw10gcc\bsp_RSc_K20\Sources" %%f in (*.h) do copy %%f "%OUTPUTDIR%\Sources\"

Copying files not working:

for /R "%ROOTDIR%\mqx\build\cw10gcc\MembrasensV1\Generated_Code" %%f in (*.h) do copy %%f "%OUTPUTDIR%\Generated_Code\"

for /R "%ROOTDIR%\mqx\build\cw10gcc\MembrasensV1\Sources" %%f in (*.h) do copy %%f "%OUTPUTDIR%\Sources\"

--------------------- ANSWER ------------------

Ok while writing this i found the mistake. It's a typo.

I forgot to put bsp_ in front of the above mentioned path.

This must have happened while copying the whole .bat file from the previously ported BSP.

The name of the BSP is in the whole .bat file w/o bsp_ and only there with bsp_ .

I just was not careful enough while changing the names.

Anyway. Thanks again.

cheers

在原帖中查看解决方案

0 项奖励
回复
2 回复数
985 次查看
danielchen
NXP TechSupport
NXP TechSupport

Hi

I think you can check the post build scripts file for your board

Let's take twrk64f120m for example

C:\Freescale\Freescale_MQX_4_2\mqx\build\bat\bsp_twrk64f120m.bat

...

copy "%ROOTDIR%\mqx\source\bsp\twrk64f120m\PE_LDD.h" "%OUTPUTDIR%\Generated_Code\PE_LDD.h" /Y

copy "%ROOTDIR%\mqx\source\bsp\twrk64f120m\PE_Types.h" "%OUTPUTDIR%\Generated_Code\PE_Types.h" /Y

....

Regards

Daniel

0 项奖励
回复
986 次查看
demheld
Contributor I

Hi

Thanks for the answer.

Those two commandlines are there and also the files are copied.

On top of that I even have the two lines which shoud exactly copy my desired files:

It is a bit strange because with one of my ported BSPs it is working and with one it's not, even though it looks good to me in

both cases.

Copying files is working:

for /R "%ROOTDIR%\mqx\build\cw10gcc\bsp_RSc_K20\Generated_Code" %%f in (*.h) do copy %%f "%OUTPUTDIR%\Generated_Code\"

for /R "%ROOTDIR%\mqx\build\cw10gcc\bsp_RSc_K20\Sources" %%f in (*.h) do copy %%f "%OUTPUTDIR%\Sources\"

Copying files not working:

for /R "%ROOTDIR%\mqx\build\cw10gcc\MembrasensV1\Generated_Code" %%f in (*.h) do copy %%f "%OUTPUTDIR%\Generated_Code\"

for /R "%ROOTDIR%\mqx\build\cw10gcc\MembrasensV1\Sources" %%f in (*.h) do copy %%f "%OUTPUTDIR%\Sources\"

--------------------- ANSWER ------------------

Ok while writing this i found the mistake. It's a typo.

I forgot to put bsp_ in front of the above mentioned path.

This must have happened while copying the whole .bat file from the previously ported BSP.

The name of the BSP is in the whole .bat file w/o bsp_ and only there with bsp_ .

I just was not careful enough while changing the names.

Anyway. Thanks again.

cheers

0 项奖励
回复