Getting serial out in CW 10.2 and MQX 3.8

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Getting serial out in CW 10.2 and MQX 3.8

Jump to solution
1,450 Views
intevac_coder
Contributor III

Hello!

What changes need to be made to get the K40 tower to output serial data to the serial port card so I can read the data stream in Hyperterminal?  I had this all fixed up in MQX 3.7 but that doesn't seem to work in 3.8.

 

I've changed user_config.h

 BSPCFG_ENABLE_TTYD 1

 

and changed twrk40x256.h

#ifndef BSP_DEFAULT_IO_CHANNEL
#if BSPCFG_ENABLE_TTYA
//#define BSP_DEFAULT_IO_CHANNEL "ttya:" /* OSJTAG-COM polled mode */
#define BSP_DEFAULT_IO_CHANNEL "ttyd:" // Tower serial polled mode
#define BSP_DEFAULT_IO_CHANNEL_DEFINED
#else
//#define BSP_DEFAULT_IO_CHANNEL NULL
#endif
#endif

 

It's always a challenge to get this running again. Thanks!

0 Kudos
Reply
1 Solution
1,046 Views
c0170
Senior Contributor III

Hi intevac coder,

 

it is the same procedure as in 3.7 to set the default IO channel.

If you did not set TTYA, then your TTYD channel was not set as default because your condition is #if BSPCFG_ENABLE_TTYA.

With correction:

#ifndef BSP_DEFAULT_IO_CHANNEL
#if BSPCFG_ENABLE_TTYD
#define BSP_DEFAULT_IO_CHANNEL "ttyd:" // Tower serial polled mode
#define BSP_DEFAULT_IO_CHANNEL_DEFINED
#else
#define BSP_DEFAULT_IO_CHANNEL NULL
#endif
#endif

 

Regards,

MartinK

View solution in original post

0 Kudos
Reply
2 Replies
1,047 Views
c0170
Senior Contributor III

Hi intevac coder,

 

it is the same procedure as in 3.7 to set the default IO channel.

If you did not set TTYA, then your TTYD channel was not set as default because your condition is #if BSPCFG_ENABLE_TTYA.

With correction:

#ifndef BSP_DEFAULT_IO_CHANNEL
#if BSPCFG_ENABLE_TTYD
#define BSP_DEFAULT_IO_CHANNEL "ttyd:" // Tower serial polled mode
#define BSP_DEFAULT_IO_CHANNEL_DEFINED
#else
#define BSP_DEFAULT_IO_CHANNEL NULL
#endif
#endif

 

Regards,

MartinK

0 Kudos
Reply
1,046 Views
intevac_coder
Contributor III

MartinK,

 

Thanks, that change worked.

0 Kudos
Reply