Hello!
What changes need to be made to get the K40 tower to output serial data to the serial port card so I can read the data stream in Hyperterminal? I had this all fixed up in MQX 3.7 but that doesn't seem to work in 3.8.
I've changed user_config.h
BSPCFG_ENABLE_TTYD 1
and changed twrk40x256.h
#ifndef BSP_DEFAULT_IO_CHANNEL
#if BSPCFG_ENABLE_TTYA
//#define BSP_DEFAULT_IO_CHANNEL "ttya:" /* OSJTAG-COM polled mode */
#define BSP_DEFAULT_IO_CHANNEL "ttyd:" // Tower serial polled mode
#define BSP_DEFAULT_IO_CHANNEL_DEFINED
#else
//#define BSP_DEFAULT_IO_CHANNEL NULL
#endif
#endif
It's always a challenge to get this running again. Thanks!
Solved! Go to Solution.
Hi intevac coder,
it is the same procedure as in 3.7 to set the default IO channel.
If you did not set TTYA, then your TTYD channel was not set as default because your condition is #if BSPCFG_ENABLE_TTYA.
With correction:
#ifndef BSP_DEFAULT_IO_CHANNEL
#if BSPCFG_ENABLE_TTYD
#define BSP_DEFAULT_IO_CHANNEL "ttyd:" // Tower serial polled mode
#define BSP_DEFAULT_IO_CHANNEL_DEFINED
#else
#define BSP_DEFAULT_IO_CHANNEL NULL
#endif
#endif
Regards,
MartinK
Hi intevac coder,
it is the same procedure as in 3.7 to set the default IO channel.
If you did not set TTYA, then your TTYD channel was not set as default because your condition is #if BSPCFG_ENABLE_TTYA.
With correction:
#ifndef BSP_DEFAULT_IO_CHANNEL
#if BSPCFG_ENABLE_TTYD
#define BSP_DEFAULT_IO_CHANNEL "ttyd:" // Tower serial polled mode
#define BSP_DEFAULT_IO_CHANNEL_DEFINED
#else
#define BSP_DEFAULT_IO_CHANNEL NULL
#endif
#endif
Regards,
MartinK
MartinK,
Thanks, that change worked.