Forcing 10 Mbps Ethernet Connection

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Forcing 10 Mbps Ethernet Connection

ソリューションへジャンプ
2,400件の閲覧回数
rdazcal
Contributor III

Greetings,

 

Is there a parameter where I can force RTCS to establish a 10 Mbps (10Base-T) even if the network supports 100 Mbps connections (100Base-TX)?

 

Also, if I do so, are there 100Base-TX only networks? I suppose a 10Base-T should work in any network, correct?

 

I need this in order to save power in my end-device

 

Thank you

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
1,627件の閲覧回数
rdazcal
Contributor III

If anyone is interested, here is a link for the solution in another thread: https://community.freescale.com/thread/72070

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,628件の閲覧回数
rdazcal
Contributor III

If anyone is interested, here is a link for the solution in another thread: https://community.freescale.com/thread/72070

0 件の賞賛
返信