Forcing 10 Mbps Ethernet Connection

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Forcing 10 Mbps Ethernet Connection

Jump to solution
2,405 Views
rdazcal
Contributor III

Greetings,

 

Is there a parameter where I can force RTCS to establish a 10 Mbps (10Base-T) even if the network supports 100 Mbps connections (100Base-TX)?

 

Also, if I do so, are there 100Base-TX only networks? I suppose a 10Base-T should work in any network, correct?

 

I need this in order to save power in my end-device

 

Thank you

Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
1,632 Views
rdazcal
Contributor III

If anyone is interested, here is a link for the solution in another thread: https://community.freescale.com/thread/72070

View solution in original post

0 Kudos
Reply
1 Reply
1,633 Views
rdazcal
Contributor III

If anyone is interested, here is a link for the solution in another thread: https://community.freescale.com/thread/72070

0 Kudos
Reply