FlexTimer(FTM) using MQX

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

FlexTimer(FTM) using MQX

跳至解决方案
2,989 次查看
freescale_sid
Contributor I

Hi,

 

         I am using K60N512 and MQX 3.8. want to use the FlexTimer(FTM) module in Quadrature Decoder Mode. I am suprised to find that there MQX code  twrk60n512 does not even contain the register definition for the Flextimer let alone any example code.

 

Can anyone please let me know how to use the Flextimer module and if someone could provide an example ?

 

As I am looking more into the MQX I am finding it difficult to use with very poor documentation and example codes. I also notice that it takes days for them to reply to your questions and even the activity by freescale on the forums is very slow. I think they should learn from the TI's Stellaris forums.

 

Regards,

Syed

 

0 项奖励
回复
1 解答
1,515 次查看
petr_uhlir
NXP Employee
NXP Employee

Hallo Robert,

The FTM is quite complex device which can be used in many different ways. That is the reason why the MQX does not contain driver for it. But the Processor Expert contains FTM driver. It embedded in TimerUnit_LDD component where you have to select FTMx_CNT as Counter. See attached screenshots from PE where FTM is used to generate PWM signal.

 

The other option is to take inspiration and reuse code from some motor control reference design

 

The 3-phase PMSM Vector Control using Quadrature Encoder on Kinetis K40

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=RD3PHASEPMSMVCQE

uses FTM for 3phase PWM generation as well as decoding quadrature signals from encoder.

 

Regards Petr

在原帖中查看解决方案

0 项奖励
回复
3 回复数
1,515 次查看
Symbolic
Contributor III

The latest CW 10.2 and MQX 3.8.1 (I don't know when it actually happened, or if it has always been there) incorporates the correct header files (for the K60, anyway) to have all the register defines and the accessors "just be there".

They actually live in MK60F15.h (in my system - which uses the K60F120M tower board).

I just generated an MQX project, and started using the structures and accessors.

My project will be using the FTM module and the eDMA module in conjunction with each other.

0 项奖励
回复
1,515 次查看
unmannedrussery
Contributor II

I recently came to this same realization - I don't believe there are any off-the-shelf MQX drivers for the Kinetis FTM. I figured I could use Processor Expert to generate some drivers that would work, but it looks like Processor Expert doesn't support the FTM module on my processor either.

 

I've decided just to buckle down and start writing my own MQX FTM drivers from scratch... in theory it shouldn't be that difficult. I'll let you know how it works out and if I have any other insights along the way.

 

Regards,

Robert

0 项奖励
回复
1,516 次查看
petr_uhlir
NXP Employee
NXP Employee

Hallo Robert,

The FTM is quite complex device which can be used in many different ways. That is the reason why the MQX does not contain driver for it. But the Processor Expert contains FTM driver. It embedded in TimerUnit_LDD component where you have to select FTMx_CNT as Counter. See attached screenshots from PE where FTM is used to generate PWM signal.

 

The other option is to take inspiration and reuse code from some motor control reference design

 

The 3-phase PMSM Vector Control using Quadrature Encoder on Kinetis K40

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=RD3PHASEPMSMVCQE

uses FTM for 3phase PWM generation as well as decoding quadrature signals from encoder.

 

Regards Petr

0 项奖励
回复