Flash Translation Layer

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Flash Translation Layer

Jump to solution
5,936 Views
v_k
Contributor I

I recently downloaded the MQX 4.0 release, and the release notes refer to availability of a flash translation layer (FTL) in the new version. The release notes say that this is available as a separate package. I haven't been able to locate it on freescale's website. Any idea when it is planned for release?

Labels (1)
Tags (2)
0 Kudos
Reply
1 Solution
3,986 Views
c0170
Senior Contributor III

Hello all,

if you haven't noticed, macl published new post with link to download NAND Flash file system, please check out the link:

NAND Flash File System patch for Freescale MQX™ RTOS 4.0.0

Regards,

MartinK

View solution in original post

0 Kudos
Reply
5 Replies
3,986 Views
DavidS
NXP Employee
NXP Employee

Hi V.K.,

MQX has a flash driver called FlashX that is used to access the on-chip flash for the various supported MCU's.

You can look at example:

C:\Freescale\Freescale_MQX_4_0\mqx\examples\flashx

You can look at the driver source code:

C:\Freescale\Freescale_MQX_4_0\mqx\source\io\flashx\freescale

Or download the baremetal Flash Drivers from web:

C90TFS_FLASH_DRIVER: TFS Flash Driver Software for Kinetis and ColdFire+ Microcontrollers.

Size (K): 9687 Format: exe Rev #: 0.3.3 Modified: 10/17/2012

Hope this helps.

Regards,

David

0 Kudos
Reply
3,986 Views
v_k
Contributor I

Hi David,

I'm looking for a flash translation layer for external NAND/NOR flash memories and then host MFS or any other file system on top of it.

Regards,

VK

0 Kudos
Reply
3,986 Views
c0170
Senior Contributor III

Hello v.k,

it has not been published on our website yet.

Regards,

MartinK

0 Kudos
Reply
3,986 Views
firebrizz
Contributor II

Hello Kojto,

you have any info about the release date?

3,987 Views
c0170
Senior Contributor III

Hello all,

if you haven't noticed, macl published new post with link to download NAND Flash file system, please check out the link:

NAND Flash File System patch for Freescale MQX™ RTOS 4.0.0

Regards,

MartinK

0 Kudos
Reply