Flash Programming using Ethernet

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Flash Programming using Ethernet

971件の閲覧回数
utsavikalpesh
Contributor V

Hi,

I am working with TWRK60D100M kit using Codewarrior v10.6 and of mqx v4.0.

Rightnow, I am using USB Multilink universal to download code.

Now my requirement is to download a code using Ethernet Cable.

Can anybody tell me what exactly I need to do???

0 件の賞賛
返信
1 返信

854件の閲覧回数
soledad
NXP Employee
NXP Employee

Hello,

You can use an Ethernet bootloader, please check the below application note:

http://cache.freescale.com/files/microcontrollers/doc/app_note/AN4367.pdf

This document describes how to use an Ethernet bootloader provided by Freescale. It explains how to modify the .lcf and .icf link files of CW and IAR IDEs respectively, in order to add the Ethernet bootloader support for your application.

In addition please check the below link: (Green Hills Probe:)

Hardware Debuggers and Programming Interfaces|Freescale


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信