Flash Programming using Ethernet

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Flash Programming using Ethernet

994 Views
utsavikalpesh
Contributor V

Hi,

I am working with TWRK60D100M kit using Codewarrior v10.6 and of mqx v4.0.

Rightnow, I am using USB Multilink universal to download code.

Now my requirement is to download a code using Ethernet Cable.

Can anybody tell me what exactly I need to do???

0 Kudos
Reply
1 Reply

877 Views
soledad
NXP Employee
NXP Employee

Hello,

You can use an Ethernet bootloader, please check the below application note:

http://cache.freescale.com/files/microcontrollers/doc/app_note/AN4367.pdf

This document describes how to use an Ethernet bootloader provided by Freescale. It explains how to modify the .lcf and .icf link files of CW and IAR IDEs respectively, in order to add the Ethernet bootloader support for your application.

In addition please check the below link: (Green Hills Probe:)

Hardware Debuggers and Programming Interfaces|Freescale


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply