[FNET/RTCS] MAC<->PHY ===> MAC<->MAC

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

[FNET/RTCS] MAC<->PHY ===> MAC<->MAC

ソリューションへジャンプ
2,303件の閲覧回数
master_szumi
Contributor III

I'm using FNET bootloader and MQX with RTCS on K60 tower and ethernet works fine.

 

I need to change PHY device (ksz8041nl on tower board) to switch device (KSZ8863RLL) so it means change MAC(K60)<->PHY to MAC(K60)<->MAC connection, I think.

 

I wonder if is it difficult to change firmware of FNET and RTCS to work properly with this hardware change?

 

 

0 件の賞賛
返信
1 解決策
1,437件の閲覧回数
drummer
Contributor IV

I am using both KSZ8041 and KSZ8873 and they both work with the same firmware.

I am using a MCF52259 and I modified the BSP by using the DEMO board example on the EVB platform.

There is no files for the KSZ8873 but it is very similar to the KSZ8041 so it works.

In the future I would like to add the additional features of the switch.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,438件の閲覧回数
drummer
Contributor IV

I am using both KSZ8041 and KSZ8873 and they both work with the same firmware.

I am using a MCF52259 and I modified the BSP by using the DEMO board example on the EVB platform.

There is no files for the KSZ8873 but it is very similar to the KSZ8041 so it works.

In the future I would like to add the additional features of the switch.

0 件の賞賛
返信