[FNET/RTCS] MAC<->PHY ===> MAC<->MAC

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

[FNET/RTCS] MAC<->PHY ===> MAC<->MAC

Jump to solution
2,298 Views
master_szumi
Contributor III

I'm using FNET bootloader and MQX with RTCS on K60 tower and ethernet works fine.

 

I need to change PHY device (ksz8041nl on tower board) to switch device (KSZ8863RLL) so it means change MAC(K60)<->PHY to MAC(K60)<->MAC connection, I think.

 

I wonder if is it difficult to change firmware of FNET and RTCS to work properly with this hardware change?

 

 

0 Kudos
Reply
1 Solution
1,432 Views
drummer
Contributor IV

I am using both KSZ8041 and KSZ8873 and they both work with the same firmware.

I am using a MCF52259 and I modified the BSP by using the DEMO board example on the EVB platform.

There is no files for the KSZ8873 but it is very similar to the KSZ8041 so it works.

In the future I would like to add the additional features of the switch.

View solution in original post

0 Kudos
Reply
1 Reply
1,433 Views
drummer
Contributor IV

I am using both KSZ8041 and KSZ8873 and they both work with the same firmware.

I am using a MCF52259 and I modified the BSP by using the DEMO board example on the EVB platform.

There is no files for the KSZ8873 but it is very similar to the KSZ8041 so it works.

In the future I would like to add the additional features of the switch.

0 Kudos
Reply