FFS nand flash demo fails during initialization

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FFS nand flash demo fails during initialization

854件の閲覧回数
visakhanc
Contributor III

Hi all,

   I have built MQX 3.8 FFS library and demo project for executing on an MPC5125 custom board. When I typed 'fsopen' shell command for initializing  the file system, It gets unresponsive. With printf debugging, I found that it stops right after this line in Media_init() function: (file: ffs\source\wearleveling\ddi_ldl\ddi_ldl_init.cpp)

   

LogicalMedia * media = new nand::Media();

The new operator does not return. So is it something related to memory allocation? I have run the MQX cplus example project without any error. Is there something specific in the FFS library or demo project that I need to change for the MPC5125 platform, like linker file settings for proper C++ operation?

Thanks for any help

ラベル(1)
タグ(4)
0 件の賞賛
返信
0 返答(返信)