FFS nand flash demo fails during initialization

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FFS nand flash demo fails during initialization

868 Views
visakhanc
Contributor III

Hi all,

   I have built MQX 3.8 FFS library and demo project for executing on an MPC5125 custom board. When I typed 'fsopen' shell command for initializing  the file system, It gets unresponsive. With printf debugging, I found that it stops right after this line in Media_init() function: (file: ffs\source\wearleveling\ddi_ldl\ddi_ldl_init.cpp)

   

LogicalMedia * media = new nand::Media();

The new operator does not return. So is it something related to memory allocation? I have run the MQX cplus example project without any error. Is there something specific in the FFS library or demo project that I need to change for the MPC5125 platform, like linker file settings for proper C++ operation?

Thanks for any help

Labels (1)
Tags (4)
0 Kudos
Reply
0 Replies