Ethernet external loopback test

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Ethernet external loopback test

1,972件の閲覧回数
Davisg
Contributor III

I need to create an Ethernet external loopback test in MQX. The test needs to work with TX+/RX+ and TX-/RX- connected externally on a 10/100 port. Is there any example code that does this in MQX?

2 返答(返信)

1,469件の閲覧回数
Davisg
Contributor III

Garabo,

I ended up moving the Ethernet external loopback test to the FNET bootloader.

Thanks

Greg

0 件の賞賛
返信

1,469件の閲覧回数
Luis_Garabo
NXP TechSupport
NXP TechSupport

Hi Greg,

What you are trying to accomplish is more a low level driver test. In the function MACNET_initialize() from MQX driver. Perhaps you can activate this option in the flags for the enet_ptr->PARAM_PTR->OPTIONS variable. Try changing this in the structure ENET_default_params[] (init_enet.c) in the 3rd element.

We don't test the loopback feature so I am not sure if this change will allow you to fully test it.

Hope this helps.

Regards,

Garabo