Ethernet external loopback test

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Ethernet external loopback test

2,008 Views
Davisg
Contributor III

I need to create an Ethernet external loopback test in MQX. The test needs to work with TX+/RX+ and TX-/RX- connected externally on a 10/100 port. Is there any example code that does this in MQX?

2 Replies

1,505 Views
Davisg
Contributor III

Garabo,

I ended up moving the Ethernet external loopback test to the FNET bootloader.

Thanks

Greg

0 Kudos
Reply

1,505 Views
Luis_Garabo
NXP TechSupport
NXP TechSupport

Hi Greg,

What you are trying to accomplish is more a low level driver test. In the function MACNET_initialize() from MQX driver. Perhaps you can activate this option in the flags for the enet_ptr->PARAM_PTR->OPTIONS variable. Try changing this in the structure ENET_default_params[] (init_enet.c) in the 3rd element.

We don't test the loopback feature so I am not sure if this change will allow you to fully test it.

Hope this helps.

Regards,

Garabo