Error: 'listensock' undeclared (first use in this function) eds.c

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Error: 'listensock' undeclared (first use in this function) eds.c

870 次查看
cencongsu
Contributor I

I try to compile the MQX 4.0.2, but I face an error:

pastedImage_0.png

I search the whole project, there is no definition for this variable: "listensock",

So , what is going on now?  Is it a bug for this version of MQX?

0 项奖励
回复
1 回复

805 次查看
soledad
NXP Employee
NXP Employee

Hello,

Before you compile your project you need to build the below libraries:

BSP, PSP, RTCS, Shell, MFS and USB.

Which device are you using?

Which project are you using?


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复