Error: 'listensock' undeclared (first use in this function) eds.c

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Error: 'listensock' undeclared (first use in this function) eds.c

843件の閲覧回数
cencongsu
Contributor I

I try to compile the MQX 4.0.2, but I face an error:

pastedImage_0.png

I search the whole project, there is no definition for this variable: "listensock",

So , what is going on now?  Is it a bug for this version of MQX?

0 件の賞賛
返信
1 返信

778件の閲覧回数
soledad
NXP Employee
NXP Employee

Hello,

Before you compile your project you need to build the below libraries:

BSP, PSP, RTCS, Shell, MFS and USB.

Which device are you using?

Which project are you using?


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信