Error Code: Out of Memory (0x0004), State Blocked

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Error Code: Out of Memory (0x0004), State Blocked

1,806 Views
MWMinor
Contributor V

I have an MQX4.1 application running under Codewarrior V10.6 on a K60 processor. It's a custom card and we're using the USB port as a device to connect the equipment to a PC.

The PC isn't connected at the moment and the application runs for varying amounts of time - 5 minutes to hours, but will suddenly stop. Not all the tasks running on the processor have stopped and after some probing we can see the USB task has thrown an error indicating it is out of memory.

TASK_TEMPLATE_STRUCT MQX_template_list[] =
{
/* Task number, Entry point, Stack, Pri, String, Auto? */
{MAIN_TASK, Main_task, 2000, 9, "main", MQX_AUTO_START_TASK},
{MENU_TASK, Menu_task, 2000, 9, "menu", 0},
{READ_TASK, Read_task, 2000, 9, "read", 0},//Reads from the touch screen
{ USB_MAIN_TASK, USB_Main_Task, 2*3000L, 9, "USBMainTask", 0, 0, 0},
{ SDCARD_TASK, sdcard_task, 2000, 11, "SDcard", MQX_AUTO_START_TASK, 0, 0 },
{READ_TASK2, read_task2, 2000, 9, "readtask2",0, 0, 0},
{0, 0, 0, 0, 0, 0, }
};

I've checked the size of the stack and usage is about 6% - so should be ok there I think...?

It's not a "heavy application" in total there are 5 or 6 tasks running, but when the system seems to halt - it invariably tracks back to the USB, so I'm thinking we're doing something wrong there.

Has anyone else seen this problem or have any ideas....?

Ken

0 Kudos
Reply
1 Reply

1,667 Views
danielchen
NXP TechSupport
NXP TechSupport

Maybe there is a memory issue in the usb task. If you only run the usb task, will you get the same error?

Regards

Daniel

0 Kudos
Reply