Error Code: Out of Memory (0x0004), State Blocked

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Error Code: Out of Memory (0x0004), State Blocked

2,363 次查看
MWMinor
Contributor V

I have an MQX4.1 application running under Codewarrior V10.6 on a K60 processor. It's a custom card and we're using the USB port as a device to connect the equipment to a PC.

The PC isn't connected at the moment and the application runs for varying amounts of time - 5 minutes to hours, but will suddenly stop. Not all the tasks running on the processor have stopped and after some probing we can see the USB task has thrown an error indicating it is out of memory.

TASK_TEMPLATE_STRUCT MQX_template_list[] =
{
/* Task number, Entry point, Stack, Pri, String, Auto? */
{MAIN_TASK, Main_task, 2000, 9, "main", MQX_AUTO_START_TASK},
{MENU_TASK, Menu_task, 2000, 9, "menu", 0},
{READ_TASK, Read_task, 2000, 9, "read", 0},//Reads from the touch screen
{ USB_MAIN_TASK, USB_Main_Task, 2*3000L, 9, "USBMainTask", 0, 0, 0},
{ SDCARD_TASK, sdcard_task, 2000, 11, "SDcard", MQX_AUTO_START_TASK, 0, 0 },
{READ_TASK2, read_task2, 2000, 9, "readtask2",0, 0, 0},
{0, 0, 0, 0, 0, 0, }
};

I've checked the size of the stack and usage is about 6% - so should be ok there I think...?

It's not a "heavy application" in total there are 5 or 6 tasks running, but when the system seems to halt - it invariably tracks back to the USB, so I'm thinking we're doing something wrong there.

Has anyone else seen this problem or have any ideas....?

Ken

0 项奖励
回复
1 回复

2,224 次查看
danielchen
NXP TechSupport
NXP TechSupport

Maybe there is a memory issue in the usb task. If you only run the usb task, will you get the same error?

Regards

Daniel

0 项奖励
回复