Does MQX for KSDK 1.0 (Beta) support using MFS to access a filesystem on an SD CARD?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Does MQX for KSDK 1.0 (Beta) support using MFS to access a filesystem on an SD CARD?

Jump to solution
1,420 Views
timothydavison
Contributor I

I'm trying to set up an FTP server on the TWR-K64 which reads/writes to a filesystem on an SD card. Is that possible with the current Beta of MQX for KSDK?  Will it be possible when the non-beta version is released in Dec?

The documentation I've found so far leads me to think this is not currently supported because the nio subsystem does not provide a driver for the SD card. Or am I missing something?

Thanks

-Tim

Labels (1)
Tags (4)
0 Kudos
Reply
1 Solution
1,129 Views
Carlos_Musich
NXP Employee
NXP Employee

Hi Timothy,

Not right now but it is planned in KSDK1.1. Please see Table 1 File systems in KSDK in C:\Freescale\MQX_KSDK_1.0.0\rtos\mqx\Getting Started with Freescale MQX RTOS for Kinetis SDK.pdf

Regards,

Carlos

View solution in original post

0 Kudos
Reply
2 Replies
1,130 Views
Carlos_Musich
NXP Employee
NXP Employee

Hi Timothy,

Not right now but it is planned in KSDK1.1. Please see Table 1 File systems in KSDK in C:\Freescale\MQX_KSDK_1.0.0\rtos\mqx\Getting Started with Freescale MQX RTOS for Kinetis SDK.pdf

Regards,

Carlos

0 Kudos
Reply
1,129 Views
timothydavison
Contributor I

Thanks for the reply.

0 Kudos
Reply