Does MQX RTOS 4.2 support USB audio class 2.0 (UAC2.0) ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Does MQX RTOS 4.2 support USB audio class 2.0 (UAC2.0) ?

Jump to solution
2,325 Views
keres_kim
Contributor II

Hi ~ community.

Glad to see MQX rtos and community members.

Does MQX RTOS 4.2 support USB audio class 2.0 (UAC2.0) ? 

It is a simple question. if someone know, please answer that question and save my time.

thank you.

Labels (1)
0 Kudos
Reply
1 Solution
2,030 Views
soledad
NXP Employee
NXP Employee

Hello keres kim,

MQX 4.2 only supports USB audio class 1.0.

However MQX for KSDK supports USB audio class 2.0.


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

2 Replies
2,031 Views
soledad
NXP Employee
NXP Employee

Hello keres kim,

MQX 4.2 only supports USB audio class 1.0.

However MQX for KSDK supports USB audio class 2.0.


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

2,030 Views
keres_kim
Contributor II

Dear Soledad,

Sounds great !!

Thank you for your response.