Does MQX RTOS 4.2 support USB audio class 2.0 (UAC2.0) ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Does MQX RTOS 4.2 support USB audio class 2.0 (UAC2.0) ?

ソリューションへジャンプ
1,484件の閲覧回数
keres_kim
Contributor II

Hi ~ community.

Glad to see MQX rtos and community members.

Does MQX RTOS 4.2 support USB audio class 2.0 (UAC2.0) ? 

It is a simple question. if someone know, please answer that question and save my time.

thank you.

ラベル(1)
タグ(2)
0 件の賞賛
返信
1 解決策
1,189件の閲覧回数
soledad
NXP Employee
NXP Employee

Hello keres kim,

MQX 4.2 only supports USB audio class 1.0.

However MQX for KSDK supports USB audio class 2.0.


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

2 返答(返信)
1,190件の閲覧回数
soledad
NXP Employee
NXP Employee

Hello keres kim,

MQX 4.2 only supports USB audio class 1.0.

However MQX for KSDK supports USB audio class 2.0.


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,189件の閲覧回数
keres_kim
Contributor II

Dear Soledad,

Sounds great !!

Thank you for your response.