Custom board with MQX 4.1 on Codewarrior 10.5

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Custom board with MQX 4.1 on Codewarrior 10.5

跳至解决方案
1,632 次查看
oscargarciaabad
Contributor III

Hello,

My Name is Oscar and I'm trying to create a Project for my custom borad using MQX 4.1. I'm using codewarrior 10.5.

I clone the TWR-K60F120M (it suits to my custom board pretty well). The cloning process is done using the clone wizard from freescale (installed with MQX 4.1). There are no problems on the process itself, and after the process is done I can build the libraries with no problems. But when I want to creata a new MQX 4.1 project for my custom board, it does not appear in the list of available devices.

What I did wrong? How can I solve that?

Thanks in advances!

Oscar.

0 项奖励
回复
1 解答
1,370 次查看
weapon
Senior Contributor I

Hi Oscar,

please refer to https://community.freescale.com/message/356271#356271

I think that may be helpful.

B.R

XWP

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,371 次查看
weapon
Senior Contributor I

Hi Oscar,

please refer to https://community.freescale.com/message/356271#356271

I think that may be helpful.

B.R

XWP

0 项奖励
回复
1,370 次查看
oscargarciaabad
Contributor III

Hi  Weiping Xu,

It worked.

Many thanks.

Oscar

0 项奖励
回复