MQX usb Device stack Vbus ISR Configuration

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MQX usb Device stack Vbus ISR Configuration

1,009件の閲覧回数
panks
Contributor I

Hi,

I have used the mqx usb device stack for my usb application. I have used IRQ6 pin interrupt to detect vbus attached event , with the help of mqx gpio example code of mcf54418 stack.

My question is that,

When I am plugging In usb connector, the interrupt comes and control goes to ISR function but it continuously cal ISR after i have removed usb connector. I have set  EPFR resigister bit in ISR using till no effect.

Where should i am wrong? Which register I have to configure in ISR so that ISR cal only one time.

Regards,

Panks

ラベル(1)
0 件の賞賛
返信
0 返答(返信)