Coverity Issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Coverity Issue

1,611 Views
divijakatabathu
Contributor I

Hi, I just need a clarification regarding the coverity issue:PW.INCLUDE_RECURSION. The MQX header file is including the header file which includes the same MQX header file inturn. So the header file is getting included recursively. Now will be there any effect in functionality if the MQX header file is excluded from the second header file.

Please suggest. Thanks in advance.

0 Kudos
Reply
1 Reply

1,380 Views
soledad
NXP Employee
NXP Employee

Hello,


Could you please let me know the name of the file you mention and include the path of this file?

Or is it possible to add a screenshot??


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply