Coverity Issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Coverity Issue

1,606件の閲覧回数
divijakatabathu
Contributor I

Hi, I just need a clarification regarding the coverity issue:PW.INCLUDE_RECURSION. The MQX header file is including the header file which includes the same MQX header file inturn. So the header file is getting included recursively. Now will be there any effect in functionality if the MQX header file is excluded from the second header file.

Please suggest. Thanks in advance.

0 件の賞賛
返信
1 返信

1,375件の閲覧回数
soledad
NXP Employee
NXP Employee

Hello,


Could you please let me know the name of the file you mention and include the path of this file?

Or is it possible to add a screenshot??


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信