Change RST of sim card slot failed...

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Change RST of sim card slot failed...

1,196 次查看
philipwang001
Contributor I

kernel: linux4.1.15

platform: imx7d

Modified DTS file, to change "MX7D_PAD_EPDC_DATA10__SIM1_PORT1_RST_B" of sim1 to be other PINs, such as "MX7D_PAD_EPDC_DATA02__GPIO2_IO2". It did not work, WHY? Is this illegal?

0 项奖励
回复
1 回复

1,084 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Wells

one can check if this pad is used by other module and in uboot.

Also one can check iomux settings with jtag to see which module owns pad.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复