Change RST of sim card slot failed...

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Change RST of sim card slot failed...

483 Views
philipwang001
Contributor I

kernel: linux4.1.15

platform: imx7d

Modified DTS file, to change "MX7D_PAD_EPDC_DATA10__SIM1_PORT1_RST_B" of sim1 to be other PINs, such as "MX7D_PAD_EPDC_DATA02__GPIO2_IO2". It did not work, WHY? Is this illegal?

0 Kudos
1 Reply

371 Views
igorpadykov
NXP Employee
NXP Employee

Hi Wells

one can check if this pad is used by other module and in uboot.

Also one can check iomux settings with jtag to see which module owns pad.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos