Cannot Save Board Configuration (BSP Cloning Wizard)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Cannot Save Board Configuration (BSP Cloning Wizard)

ソリューションへジャンプ
1,205件の閲覧回数
razed11
Contributor V

Hi,

I created a new board definition file based on the K64 FRDM. I deselect all examples and select only IAR as the IDE. At this point there is no way to save this information. If I close and reopen the application or the file everything is selected again. Not a huge problem but it seems like an oversight.

MQX 4.1.1

Thanks,

Kenny

0 件の賞賛
返信
1 解決策
1,054件の閲覧回数
RadekS
NXP Employee
NXP Employee

Thank you for your suggestion.

I agree that it will be nice and implementation should not be difficult.

I suggested this improvement to responsible designer.

I guess that it will be implemented in next versions.


Have a great day,
RadekS

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,055件の閲覧回数
RadekS
NXP Employee
NXP Employee

Thank you for your suggestion.

I agree that it will be nice and implementation should not be difficult.

I suggested this improvement to responsible designer.

I guess that it will be implemented in next versions.


Have a great day,
RadekS

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信