Cannot Save Board Configuration (BSP Cloning Wizard)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Cannot Save Board Configuration (BSP Cloning Wizard)

Jump to solution
1,225 Views
razed11
Contributor V

Hi,

I created a new board definition file based on the K64 FRDM. I deselect all examples and select only IAR as the IDE. At this point there is no way to save this information. If I close and reopen the application or the file everything is selected again. Not a huge problem but it seems like an oversight.

MQX 4.1.1

Thanks,

Kenny

0 Kudos
Reply
1 Solution
1,074 Views
RadekS
NXP Employee
NXP Employee

Thank you for your suggestion.

I agree that it will be nice and implementation should not be difficult.

I suggested this improvement to responsible designer.

I guess that it will be implemented in next versions.


Have a great day,
RadekS

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,075 Views
RadekS
NXP Employee
NXP Employee

Thank you for your suggestion.

I agree that it will be nice and implementation should not be difficult.

I suggested this improvement to responsible designer.

I guess that it will be implemented in next versions.


Have a great day,
RadekS

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply