Can the K60 running MQX 4.0 support both HTTP server and SNMPv2 at the same time

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can the K60 running MQX 4.0 support both HTTP server and SNMPv2 at the same time

1,354 Views
terrybiberdorf
Contributor II

I'm working on a project that requires both HTTP and SNMP operation at the same time.

My current configuration is a K60D100M, I'm using Code Warrior 10.4 IDE

My tool chain is MQX 4.0 GCC build.

I have separate projects running either SNMPv2c or HTTP server but when I attempt to merge the two project together they don't seem to play nice.

My sample merged project is using the HTTP sample project to establish network connection.  My project then spins off a SNMP task.  It attempts to start but fails to complete the following API: error = SNMP_init_with_traps("SNMP", 10, 3000, my_trap_list);

From what I can tell when stepping through the code, this API does not even return.

My first general question would be: Can MQX support HTTP server operation at the same time as SNMP?

Thanks

Terry

Tags (4)
0 Kudos
Reply
2 Replies

1,134 Views
thom_nic
Contributor II

Hi Terry - were you able to resolve this issue?  Looking to do something similar.  Thanks.

0 Kudos
Reply

1,134 Views
tbiberdorf
Contributor IV

I dropped MQX and moved to FreeRTOS with Interniche stack.

Our primary reason to leaving MQX was a requirement to support SNMPv3.  MQX does not support SNMPv3.