need MQX4.1.1 library for K61FX512VMJ15.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

need MQX4.1.1 library for K61FX512VMJ15.

1,325件の閲覧回数
virendrapatel
Contributor III

Hi,..

We are using MQX4.1.1 on K61FX512VMJ15.

We need library for MQX RTOS for K61FX512VMJ15.

We have generated the library from MQX cloning wiz. from base board twrk70f120m, but it is operated on 120Mhz.

We need the configure our K61 for 150Mhz.

can anybody please  provide us a MQX library for K61FX512VMJ15 with 150mhz clock configuration.

Thanks,

Virendra

タグ(2)
0 件の賞賛
返信
1 返信

1,222件の閲覧回数
soledad
NXP Employee
NXP Employee

Hello virendra,

Unfortunately we don’t have a BSP for K61 devices, it is necessary to create or clone your own BSP; however you can use the MQX BSP Cloning Wizard and use the twrk60f120m for board base. Then it is necessary to modify the pin definitions according with the K61 package. You can find the pin definitions in the init_xxxx.c files (MQX_install_path\mqx\source\bsp\twr_new_BSP).

In your case you need to change the core frecuency, for do that you need to check the “How-to Change Default Clock Settings in Kinetis BSPs” document that you can find at the path: C:\Freescale\Freescale_MQX_4_1\doc\tools\cw  (it is attached to this thread too)


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信