CPU, CORE and BUS frequencies, FNET configuration and MQX configuration

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CPU, CORE and BUS frequencies, FNET configuration and MQX configuration

Jump to solution
1,001 Views
Skyhawk
Contributor I

Hi all,

 

I'm working on the TWR-K60N512 tower, in the gettings started pdf, I read about the TWR-K60N512 board.

 

Core Clock 96 MHz
Bus Clock 48 MHz

 

However on both the TWR-K60N512 board and the TWR-SER board there are 50Mhz oscilators.

How do the external oscillator frequecies correspond to the Core and Bus frequencies?

 

Greetings,


 

 

0 Kudos
Reply
1 Solution
814 Views
c0170
Senior Contributor III

Hi Skyhawk,

 

Please check this document : K60 Reference Manual chapter 5 Clock distribution. There are located clocking diagram, clock definitions and internal clock requirements.

 

Regards,

MartinK

View solution in original post

0 Kudos
Reply
1 Reply
815 Views
c0170
Senior Contributor III

Hi Skyhawk,

 

Please check this document : K60 Reference Manual chapter 5 Clock distribution. There are located clocking diagram, clock definitions and internal clock requirements.

 

Regards,

MartinK

0 Kudos
Reply