CPU, CORE and BUS frequencies, FNET configuration and MQX configuration

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CPU, CORE and BUS frequencies, FNET configuration and MQX configuration

ソリューションへジャンプ
1,359件の閲覧回数
Skyhawk
Contributor I

Hi all,

 

I'm working on the TWR-K60N512 tower, in the gettings started pdf, I read about the TWR-K60N512 board.

 

Core Clock 96 MHz
Bus Clock 48 MHz

 

However on both the TWR-K60N512 board and the TWR-SER board there are 50Mhz oscilators.

How do the external oscillator frequecies correspond to the Core and Bus frequencies?

 

Greetings,


 

 

0 件の賞賛
返信
1 解決策
1,172件の閲覧回数
c0170
Senior Contributor III

Hi Skyhawk,

 

Please check this document : K60 Reference Manual chapter 5 Clock distribution. There are located clocking diagram, clock definitions and internal clock requirements.

 

Regards,

MartinK

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,173件の閲覧回数
c0170
Senior Contributor III

Hi Skyhawk,

 

Please check this document : K60 Reference Manual chapter 5 Clock distribution. There are located clocking diagram, clock definitions and internal clock requirements.

 

Regards,

MartinK

0 件の賞賛
返信